Part Number: TLV3601
Other Parts Discussed in Thread: LMG1020, TLV3604, PSPICE-FOR-TI, TINA-TI, , TLV3605
I attempted to use the TLV3604/3601 together with the LMG1020 to implement a low-side GaN FET driver, similar to the example provided by TI. However, even when keeping all electrical parameters identical to those used in the provided TINA example, I am still unable to obtain the correct results in ADS. The output of the TLV3604 consistently operates at a -100V common-mode level, which is clearly a mathematical simulation error.
Based on the information I found in forums, I cannot confirm whether this issue is caused by an incorrect pin numbering assignment.
Are there any possible approaches to troubleshoot this issue?