This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA838: Why is the range of the input signal in my simulation not quite the same as that in the manual?

Part Number: OPA838

Here's my schematic why I can't output a properly amplified signal when the input signal amplitude is 1.5V.

When I input a signal amplitude of 1.2V it is ok. And according to the info in the manual a 1.5V signal is not outside the normal operating range.