This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP8646: 8646的实际输出电压为2.2V左右,理应0.24V左右

Part Number: LMP8646
Other Parts Discussed in Thread: LM5122,

设计目标:限流值为5A,

背景:主电路输出电压:63V左右(T3,T4端子之间电压),Rsense=30mΩ,Rg=40kΩ,6脚供电电源:5V+。

主电路的输出电流在1A的时候,8646的实际输出电压为2.2V左右,理论值应是:0.24V,两者相差很大。

已进行过的Troubleshot:

①更换了过全新的8646,结果与之前一致(2.2V左右)。

②拆掉Cg验证,结果也与之前一致(2.2V左右)

③拆掉C27,并用0Ω电阻替换R4,R5,结果也与之前一致(2.2V左右)。

目前可以确定的是:Vsense是正确的,为:0.03V。

问题出在哪了呢?可不可以一起看下?