Part Number: OPA544
Other Parts Discussed in Thread: NE5532

我正在测试OPA544的功能,结果遇到了严重的震荡问题。以上是我的原理图,使用±18 V供电(在供电端再接对地10 uF电容后无影响),无论VIN+接什么,只要VO和VIN-连接起来(无论是直接连接还是通过一个68k的电阻连接),VO都会出现几个V的震荡,并伴随急速发热。在反馈回路中加47 pF到100 nF的电容均不会影响这一现象。无论是在面包板还是PCB板上都是同样的现象。更换了3个OPA544,均有相同情况。
此外,我还发现,当VIN+或VIN-端用导线伸出时,震荡幅度对导线的形状敏感。有时,即使VO和VIN-没有构成反馈回路,只要碰一下VIN+端的导线,在VO端也会发生震荡并伴随剧烈发热(而当用手接触to-220封装的tab时,这种震荡会得到缓解)。
请问这种情况是何原因,如何解决?