Other Parts Discussed in Thread: DRV8842
请问drv8842的文档上说的IN1,IN2,,I0~I4,DECAY,NRESET,NSLEEP管脚是不是都可以接5v的输入电平(除了vref要接3.3v)?,像下图所示,最大范围可到7V,默认是5V?
请客在Absolute Maximum Rating下的测试条件,这个下面参数是在您这个参数参考意义不大,建议您参考Recommended Operating Conditions
digital input pin支持3.3V和5V电平,最大耐压7V。
Vref最大耐压4V。