drv8301 #fault什么状态是正常的?

Other Parts Discussed in Thread: DRV8301

drv8301数据手册里写到 #fault在上电初始化的时候会拉高,同时PWM可以输出,所以我认为#fault高电平是正常的对不对?我的电机驱动,开环是正常的,电机能正常运转,测的GVDD电压为11V左右,但是我用电流模式的时候,drv8301的PWM输出没有了,应该是保护了,#fault变低,用SPI读8301的寄存器的0和1发现GVDD_UV和GVDD_OV都是1,实测GVDD处电压为0,这是怎么回事呢,是什么原因是GVDD电压变低呢? 我的PVDD为24V。