最新做了一个板子,使用了DS80PCI800芯片,芯片接法完全按照评估板的接法连接,
同时设置如下:使能内部的ldo,PRSNT=0,RXDET=F,RATE=0,SD_TH=F,RES=F,ENSMB=0,EQA/B[1:0]=00,00,DEMA/B[1:0]=FR,FR。我们使用xilinx的pcie的example_design工程测试,无法搜到PCIE设备,RATE进行不同的设置都搜不到设备。
与此同时我们使用xilinx的ibert工程测试,上述参数无法测试用过,但是将RATE=R,DEMA/B[1:0]=FF,FF的设置下是可以测试通过的,工具显示眼图也很好。
我们的板卡因为种种原因结构如下:PCIE板卡(12inch)-----转接卡(TX,RX均放置了该芯片,1inch)----连接到Xilinx FPGA板卡(5inch).
拜托工程时帮我看一下,设置上有什么问题吗?另外这个片子可以用来测试1个通道的PCIE工程吗?