Other Parts Discussed in Thread: IWR6843ISK
你好!
目前使用IWR6843ISK产品,使用的例程是out of box demo里面对应的程序68xx_mmwave_sdk_dsp,距离维256,速度维32.
1.B=Slope*256/fs=150MHz;
当Tadctime 取1133us(225.9khz), 566.5us(451.8kHz),226.6us(1129.5kHz),改变对应其他参数,都是配置不成功。
当Tadctime取113.3us可以配置成功,具体值:idletime:1378.7us ;ramptime:121.3us Tadctime:113.3us fs:2259kHz slope:1.323MHz/us
只查到6843的fs的max为12.5M,这个是不是采样频率和斜率不能设置太低?
2.对应该芯片,采用距离维512*速度维16,和256*32,哪种性能更稳定?还是效果一样?
3.detObjOutMaxSize这个值在场景中检测到(这取决于配置,如cfar阈值,*静态杂乱清除等)和内存和MIPS限制,看了一下,程序中是500,这个有具体的计算公式吗?或者相关资料吗?极限能做到多少呢?