使用iwr6843ISK运行mmwave_industrial_toolbox_4_5_1的traffic_monitoring报错,gui页面卡住,不知道是哪里有问题,使用的是原来的参数文件,没有修改。
报错如下:
COM3 opened.
COM4 opened.
警告: 目录已存在。
> In tm_visualizer (line 39)
Opening tm_demo_uart_stream.txt. Ready to log data.
Opening configuration file
Parsing configuration file...
Skip parsing for: sensorStop command
Skip parsing for: flushCfg command
Error: number of parameters is incorrect for stateParam commandError: number of parameters is incorrect for trackingCfg commandSkip parsing for: sensorPosition command
Skip parsing for: presenceBoundaryBox command
Skip parsing for: sensorStart command
COM3 opened.
COM4 opened.
Sending cfg file to device...
sensorStop
flushCfg
Done
dfeDataOutputMode 1
Done
channelCfg 15 5 0
Done
adcCfg 2 1
Done
adcbufCfg -1 0 1 1 1
Done
profileCfg 0 60 8 7 28 0 0 20 1 256 12500 0 0 48
Done
chirpCfg 0 0 0 0 0 0 0 1
Done
chirpCfg 1 1 0 0 0 0 0 4
Done
frameCfg 0 1 64 0 50 1 0
Done
lowPower 0 0
Done
guiMonitor -1 1 0 0 0 0 0
Done
cfarCfg -1 0 2 8 4 3 0 10 0
Done
cfarCfg -1 1 0 4 2 3 1 12 0
Done
multiObjBeamForming -1 1 0.5
Done
clutterRemoval -1 1
Done
calibDcRangeSig -1 0 -5 8 256
Done
extendedMaxVelocity -1 1
Done
bpmCfg -1 0 0 1
Done
lvdsStreamCfg -1 0 0 0
Done
compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
Done
measureRangeBiasAndRxChanPhase 0 1.5 0.2
Done
CQRxSatMonitor 0 3 4 63 0
Done
CQSigImgMonitor 0 127 4
Done
analogMonitor 0 0
Done
aoaFovCfg -1 -90 90 -90 90
Done
cfarFovCfg -1 0 0 80
Done
cfarFovCfg -1 1 -30 30.00
Done
staticBoundaryBox -40 40 20 70 -3 3
Done
boundaryBox -50 50 10 80 -3 3
Done
gatingParam 20 15 15 15 200
Done
stateParam 15 10 10 1000 10 1000
Done
allocationParam 60 50 1 3 5 50.0
Done
maxAcceleration 50 50 0.1
Done
trackingCfg 1 2 250 20 113 355 50
Done
sensorPosition 2 0 0
Done
presenceBoundaryBox -3 3 2 6 0.5 2.5
Done
sensorStart
Issue with Frame 40. Skipping. Expected packet length: 2080; Actual length: 4223.