TI的工程师好,我在测试一个4串锂电池保护板的电压采样方案。采用了CD4052将4串电池电压逐一传递给差分运放电路采样。该部分原理图如图所示。一开始如图测试,CD4052可以按照AB控制引脚的电平状态将X和Y口与响应的XOUT和YOUT接通,导通压降也正常。但是由于发现R65,R66,R71,R73,R76上的压降还是太大,所以我将这5个电阻全部替换为0值电阻。但是替换之后,再次接电池上电时,CD4052的通道映射就开始出现问题了,虽然依旧可以按照AB控制引脚的电平状态进行变化,但是通道接通后的电压不对。比如X0=12V,Y0=9V时,控制AB为00,而接通到XOUT=0.1V,YOUT=4V。AB为其他状态时X和Y的接通均有不同程度的输入输出差异太大的异常,唯有控制Y3=3V接到YOUT时和X1=3V接到XOUT时以及Y1=0V接到YOUT时(0V嘛,本来应该没差),输入输出接通相等。为了避免运放电路的干扰我将R51,R55和C20去掉后进行测试,问题依旧不变。似乎就是上边几个电池通道出现了异常。这之后我再将电阻换回1K但问题也依旧,请问这说明芯片上边几个通道已经损坏了吗?