drv8833两片并联驱动一个有刷直流电机

Other Parts Discussed in Thread: DRV8833

我的是有刷直流电机,供电电压是7.2V,最大功率时电流为4.2A,停止电流8A,最大效率时电流1.76A,我希望用两片drv8833并联驱动一个电机,不知道设计电路时需要注意哪些地方

  • 努力保证两芯片信号的同步,防止其中一个变成一个的负载。

  • 我的两片drv8833使用的是相同的控制信号,从同样的两根控制信号分开到两个芯片的,可是一焊接上两个芯片,电机就无法转动,只焊接一个就可以转动,估计是出现了您说的其中一个成为了另外一个的负载,可是明明是同样的信号线为什么会出现控制不同步了呢?难道是因为信号线的走线长度的差异吗?

  • 另外我想一个芯片的两个H桥可以并联驱动一个电机,那我想应该两个芯片4个H桥应该也可以啊,芯片资料上说 The two H-bridges in the DRV8833 can be connected in parallel for double the current of a single H-bridge. The internal dead time in the DRV8833 prevents any risk of cross-conduction (shoot-through) between the two bridges due to timing differences between the two bridges. The drawing below shows the connections.这里说了可以防止两个H桥之间交叉传导,那为什么到了4个H桥就不能防止这个功能了呢?是因为那个internal dead time 只能满足两个H桥的实现并联吗?