Other Parts Discussed in Thread: DRV8833
我的是有刷直流电机,供电电压是7.2V,最大功率时电流为4.2A,停止电流8A,最大效率时电流1.76A,我希望用两片drv8833并联驱动一个电机,不知道设计电路时需要注意哪些地方
另外我想一个芯片的两个H桥可以并联驱动一个电机,那我想应该两个芯片4个H桥应该也可以啊,芯片资料上说 The two H-bridges in the DRV8833 can be connected in parallel for double the current of a single H-bridge. The internal dead time in the DRV8833 prevents any risk of cross-conduction (shoot-through) between the two bridges due to timing differences between the two bridges. The drawing below shows the connections.这里说了可以防止两个H桥之间交叉传导,那为什么到了4个H桥就不能防止这个功能了呢?是因为那个internal dead time 只能满足两个H桥的实现并联吗?