现在正准备用DRV8332芯片设计三相步进电机驱动器,有几个问题请高手们帮助回复,谢谢!
1,由于整个系统的供电只有12VDC,所以DRV8332的供电PVDD=12V,GVDD=12V,VDD=12V是否可以正常工作。
2,DRV8332规格书中持续输出电流是8A,而芯片的封装各ABC各相引脚的供电及输出脚都只有一个引脚,请问一个引脚输出是否可以承受8A的电流。
3,规格书中写道:Low R these motor drivers can be up to 97%, which enables DS(on) MOSFETs (80 mΩ at TJ = 25°C),请问此Rds(on)受输出电流的影响会增大了,在持续5A输出的,Rds(on)多大呢。
谢谢!愿与大家交流!
viken@126.com
QQ:40366143