程序代码如下:
TOUCH.C程序:
#include "inc/hw_adc.h"
#include "inc/hw_gpio.h"
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_timer.h"
#include "inc/hw_types.h"
#include "driverlib/adc.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/sysctl.h"
#include "driverlib/timer.h"
#include "grlib/grlib.h"
#include "grlib/widget.h"
#include "drivers/touch.h"
//*****************************************************************************
//
// This driver operates in four different screen orientations. They are:
//
// * Portrait - The screen is taller than it is wide, and the flex connector is
// on the left of the display. This is selected by defining
// PORTRAIT.
//
// * Landscape - The screen is wider than it is tall, and the flex connector is
// on the bottom of the display. This is selected by defining
// LANDSCAPE.
//
// * Portrait flip - The screen is taller than it is wide, and the flex
// connector is on the right of the display. This is
// selected by defining PORTRAIT_FLIP.
//
// * Landscape flip - The screen is wider than it is tall, and the flex
// connector is on the top of the display. This is
// selected by defining LANDSCAPE_FLIP.
//
// These can also be imagined in terms of screen rotation; if portrait mode is
// 0 degrees of screen rotation, landscape is 90 degrees of counter-clockwise
// rotation, portrait flip is 180 degrees of rotation, and landscape flip is
// 270 degress of counter-clockwise rotation.
//
// If no screen orientation is selected, "landscape flip" mode will be used.
//
//*****************************************************************************
#if ! defined(PORTRAIT) && ! defined(PORTRAIT_FLIP) && \
! defined(LANDSCAPE) && ! defined(LANDSCAPE_FLIP)
#define LANDSCAPE_FLIP
#endif
//*****************************************************************************
//
// The GPIO pins to which the touch screen is connected.
//
//*****************************************************************************
#define TS_P_PERIPH SYSCTL_PERIPH_GPIOE
#define TS_P_BASE GPIO_PORTE_BASE
#define TS_N_PERIPH SYSCTL_PERIPH_GPIOE
#define TS_N_BASE GPIO_PORTE_BASE
#define TS_XP_PIN GPIO_PIN_6
#define TS_YP_PIN GPIO_PIN_7
#define TS_XN_PIN GPIO_PIN_2
#define TS_YN_PIN GPIO_PIN_3
//*****************************************************************************
//
// The ADC channels connected to each of the touch screen contacts.
//
//*****************************************************************************
#define ADC_CTL_CH_XP ADC_CTL_CH1
#define ADC_CTL_CH_YP ADC_CTL_CH0
//*****************************************************************************
//
// The coefficients used to convert from the ADC touch screen readings to the
// screen pixel positions.
//
//*****************************************************************************
#ifdef PORTRAIT
#define M0 480
#define M1 77856
#define M2 -22165152
#define M3 86656
#define M4 1792
#define M5 -19209728
#define M6 199628
#endif
#ifdef LANDSCAPE
#define M0 86784
#define M1 -1536
#define M2 -17357952
#define M3 -144
#define M4 -78576
#define M5 69995856
#define M6 201804
#endif
#ifdef PORTRAIT_FLIP
#define M0 -864
#define M1 -79200
#define M2 70274016
#define M3 -85088
#define M4 1056
#define M5 80992576
#define M6 199452
#endif
#ifdef LANDSCAPE_FLIP
#define M0 -83328
#define M1 1664
#define M2 78919456
#define M3 -336
#define M4 80328
#define M5 -22248408
#define M6 198065
#endif
//*****************************************************************************
//
// The current state of the touch screen driver's state machine. This is used
// to cycle the touch screen interface through the powering sequence required
// to read the two axes of the surface.
//
//*****************************************************************************
static unsigned long g_ulTSState;
#define TS_STATE_INIT 0
#define TS_STATE_READ_X 1
#define TS_STATE_READ_Y 2
#define TS_STATE_SKIP_X 3
#define TS_STATE_SKIP_Y 4
//*****************************************************************************
//
// The most recent raw ADC reading for the X position on the screen. This
// value is not affected by the selected screen orientation.
//
//*****************************************************************************
volatile short g_sTouchX;
//*****************************************************************************
//
// The most recent raw ADC reading for the Y position on the screen. This
// value is not affected by the selected screen orientation.
//
//*****************************************************************************
volatile short g_sTouchY;
//*****************************************************************************
//
// A pointer to the function to receive messages from the touch screen driver
// when events occur on the touch screen (debounced presses, movement while
// pressed, and debounced releases).
//
//*****************************************************************************
static long (*g_pfnTSHandler)(unsigned long ulMessage, long lX, long lY);
//*****************************************************************************
//
// The current state of the touch screen debouncer. When zero, the pen is up.
// When three, the pen is down. When one or two, the pen is transitioning from
// one state to the other.
//
//*****************************************************************************
static unsigned char g_cState = 0;
//*****************************************************************************
//
// The queue of debounced pen positions. This is used to slightly delay the
// returned pen positions, so that the pen positions that occur while the pen
// is being raised are not send to the application.
//
//*****************************************************************************
static short g_psSamples[8];
//*****************************************************************************
//
// The count of pen positions in g_psSamples. When negative, the buffer is
// being pre-filled as a result of a detected pen down event.
//
//*****************************************************************************
static signed char g_cIndex = 0;
//*****************************************************************************
//
//! Debounces presses of the touch screen.
//!
//! This function is called when a new X/Y sample pair has been captured in
//! order to perform debouncing of the touch screen.
//!
//! \return None.
//
//*****************************************************************************
static void
TouchScreenDebouncer(void)
{
long lX, lY, lTemp;
//
// Convert the ADC readings into pixel values on the screen.
//
lX = g_sTouchX;
lY = g_sTouchY;
lTemp = ((lX * M0) + (lY * M1) + M2) / M6;
lY = ((lX * M3) + (lY * M4) + M5) / M6;
lX = lTemp;
//
// See if the touch screen is being touched.
//
if((g_sTouchX < TOUCH_MIN) || (g_sTouchY < TOUCH_MIN))
{
//
// See if the pen is not up right now.
//
if(g_cState != 0x00)
{
//
// Decrement the state count.
//
g_cState--;
//
// See if the pen has been detected as up three times in a row.
//
if(g_cState == 0x80)
{
//
// Indicate that the pen is up.
//
g_cState = 0x00;
//
// See if there is a touch screen event handler.
//
if(g_pfnTSHandler)
{
//
// Send the pen up message to the touch screen event
// handler.
//
g_pfnTSHandler(WIDGET_MSG_PTR_UP, g_psSamples[g_cIndex],
g_psSamples[g_cIndex + 1]);
}
}
}
}
else
{
//
// See if the pen is not down right now.
//
if(g_cState != 0x83)
{
//
// Increment the state count.
//
g_cState++;
//
// See if the pen has been detected as down three times in a row.
//
if(g_cState == 0x03)
{
//
// Indicate that the pen is up.
//
g_cState = 0x83;
//
// Set the index to -8, so that the next 3 samples are stored
// into the sample buffer before sending anything back to the
// touch screen event handler.
//
g_cIndex = -8;
//
// Store this sample into the sample buffer.
//
g_psSamples[0] = lX;
g_psSamples[1] = lY;
}
}
else
{
//
// See if the sample buffer pre-fill has completed.
//
if(g_cIndex == -2)
{
//
// See if there is a touch screen event handler.
//
if(g_pfnTSHandler)
{
//
// Send the pen down message to the touch screen event
// handler.
//
g_pfnTSHandler(WIDGET_MSG_PTR_DOWN, g_psSamples[0],
g_psSamples[1]);
}
//
// Store this sample into the sample buffer.
//
g_psSamples[0] = lX;
g_psSamples[1] = lY;
//
// Set the index to the next sample to send.
//
g_cIndex = 2;
}
//
// Otherwise, see if the sample buffer pre-fill is in progress.
//
else if(g_cIndex < 0)
{
//
// Store this sample into the sample buffer.
//
g_psSamples[g_cIndex + 10] = lX;
g_psSamples[g_cIndex + 11] = lY;
//
// Increment the index.
//
g_cIndex += 2;
}
//
// Otherwise, the sample buffer is full.
//
else
{
//
// See if there is a touch screen event handler.
//
if(g_pfnTSHandler)
{
//
// Send the pen move message to the touch screen event
// handler.
//
g_pfnTSHandler(WIDGET_MSG_PTR_MOVE, g_psSamples[g_cIndex],
g_psSamples[g_cIndex + 1]);
}
//
// Store this sample into the sample buffer.
//
g_psSamples[g_cIndex] = lX;
g_psSamples[g_cIndex + 1] = lY;
//
// Increment the index.
//
g_cIndex = (g_cIndex + 2) & 7;
}
}
}
}
//*****************************************************************************
//
//! Handles the ADC interrupt for the touch screen.
//!
//! This function is called when the ADC sequence that samples the touch screen
//! has completed its acquisition. The touch screen state machine is advanced
//! and the acquired ADC sample is processed appropriately.
//!
//! It is the responsibility of the application using the touch screen driver
//! to ensure that this function is installed in the interrupt vector table for
//! the ADC3 interrupt.
//!
//! \return None.
//
//*****************************************************************************
void
TouchScreenIntHandler(void)
{
//
// Clear the ADC sample sequence interrupt.
//
HWREG(ADC0_BASE + ADC_O_ISC) = 1 << 3;
//
// Determine what to do based on the current state of the state machine.
//
switch(g_ulTSState)
{
//
// The new sample is an X axis sample that should be discarded.
//
case TS_STATE_SKIP_X:
{
//
// Read and throw away the ADC sample.
//
HWREG(ADC0_BASE + ADC_O_SSFIFO3);
//
// Set the analog mode select for the YP pin.
//
HWREG(TS_P_BASE + GPIO_O_AMSEL) =
HWREG(TS_P_BASE + GPIO_O_AMSEL) | TS_YP_PIN;
//
// Configure the Y axis touch layer pins as inputs.
//
HWREG(TS_P_BASE + GPIO_O_DIR) =
HWREG(TS_P_BASE + GPIO_O_DIR) & ~TS_YP_PIN;
HWREG(TS_N_BASE + GPIO_O_DIR) =
HWREG(TS_N_BASE + GPIO_O_DIR) & ~TS_YN_PIN;
//
// The next sample will be a valid X axis sample.
//
g_ulTSState = TS_STATE_READ_X;
//
// This state has been handled.
//
break;
}
//
// The new sample is an X axis sample that should be processed.
//
case TS_STATE_READ_X:
{
//
// Read the raw ADC sample.
//
g_sTouchX = HWREG(ADC0_BASE + ADC_O_SSFIFO3);
//
// Clear the analog mode select for the YP pin.
//
HWREG(TS_P_BASE + GPIO_O_AMSEL) =
HWREG(TS_P_BASE + GPIO_O_AMSEL) & ~TS_YP_PIN;
//
// Configure the X and Y axis touch layers as outputs.
//
HWREG(TS_P_BASE + GPIO_O_DIR) =
HWREG(TS_P_BASE + GPIO_O_DIR) | TS_XP_PIN | TS_YP_PIN;
HWREG(TS_N_BASE + GPIO_O_DIR) =
HWREG(TS_N_BASE + GPIO_O_DIR) | TS_XN_PIN | TS_YN_PIN;
//
// Drive the positive side of the Y axis touch layer with VDD and
// the negative side with GND. Also, drive both sides of the X
// axis layer with GND to discharge any residual voltage (so that
// a no-touch condition can be properly detected).
//
HWREG(TS_N_BASE + GPIO_O_DATA + ((TS_XN_PIN | TS_YN_PIN) << 2)) =
0;
HWREG(TS_P_BASE + GPIO_O_DATA + ((TS_XP_PIN | TS_YP_PIN) << 2)) =
TS_YP_PIN;
//
// Configure the sample sequence to capture the X axis value.
//
HWREG(ADC0_BASE + ADC_O_SSMUX3) = ADC_CTL_CH_XP;
//
// The next sample will be an invalid Y axis sample.
//
g_ulTSState = TS_STATE_SKIP_Y;
//
// This state has been handled.
//
break;
}
//
// The new sample is a Y axis sample that should be discarded.
//
case TS_STATE_SKIP_Y:
{
//
// Read and throw away the ADC sample.
//
HWREG(ADC0_BASE + ADC_O_SSFIFO3);
//
// Set the analog mode select for the XP pin.
//
HWREG(TS_P_BASE + GPIO_O_AMSEL) =
HWREG(TS_P_BASE + GPIO_O_AMSEL) | TS_XP_PIN;
//
// Configure the X axis touch layer pins as inputs.
//
HWREG(TS_P_BASE + GPIO_O_DIR) =
HWREG(TS_P_BASE + GPIO_O_DIR) & ~TS_XP_PIN;
HWREG(TS_N_BASE + GPIO_O_DIR) =
HWREG(TS_N_BASE + GPIO_O_DIR) & ~TS_XN_PIN;
//
// The next sample will be a valid Y axis sample.
//
g_ulTSState = TS_STATE_READ_Y;
//
// This state has been handled.
//
break;
}
//
// The new sample is a Y axis sample that should be processed.
//
case TS_STATE_READ_Y:
{
//
// Read the raw ADC sample.
//
g_sTouchY = HWREG(ADC0_BASE + ADC_O_SSFIFO3);
//
// The next configuration is the same as the initial configuration.
// Therefore, fall through into the initialization state to avoid
// duplicating the code.
//
}
//
// The state machine is in its initial state
//
case TS_STATE_INIT:
{
//
// Clear the analog mode select for the XP pin.
//
HWREG(TS_P_BASE + GPIO_O_AMSEL) =
HWREG(TS_P_BASE + GPIO_O_AMSEL) & ~TS_XP_PIN;
//
// Configure the X and Y axis touch layers as outputs.
//
HWREG(TS_P_BASE + GPIO_O_DIR) =
HWREG(TS_P_BASE + GPIO_O_DIR) | TS_XP_PIN | TS_YP_PIN;
HWREG(TS_N_BASE + GPIO_O_DIR) =
HWREG(TS_N_BASE + GPIO_O_DIR) | TS_XN_PIN | TS_YN_PIN;
//
// Drive one side of the X axis touch layer with VDD and the other
// with GND. Also, drive both sides of the Y axis layer with GND
// to discharge any residual voltage (so that a no-touch condition
// can be properly detected).
//
HWREG(TS_P_BASE + GPIO_O_DATA + ((TS_XP_PIN | TS_YP_PIN) << 2)) =
TS_XP_PIN;
HWREG(TS_N_BASE + GPIO_O_DATA + ((TS_XN_PIN | TS_YN_PIN) << 2)) =
0;
//
// Configure the sample sequence to capture the Y axis value.
//
HWREG(ADC0_BASE + ADC_O_SSMUX3) = ADC_CTL_CH_YP;
//
// If this is the valid Y sample state, then there is a new X/Y
// sample pair. In that case, run the touch screen debouncer.
//
if(g_ulTSState == TS_STATE_READ_Y)
{
TouchScreenDebouncer();
}
//
// The next sample will be an invalid X axis sample.
//
g_ulTSState = TS_STATE_SKIP_X;
//
// This state has been handled.
//
break;
}
}
}
//*****************************************************************************
//
//! Initializes the touch screen driver.
//!
//! This function initializes the touch screen driver, beginning the process of
//! reading from the touch screen. This driver uses the following hardware
//! resources:
//!
//! - ADC sample sequence 3
//! - Timer 1 subtimer A
//!
//! \return None.
//
//*****************************************************************************
void
TouchScreenInit(void)
{
//
// Set the initial state of the touch screen driver's state machine.
//
g_ulTSState = TS_STATE_INIT;
//
// There is no touch screen handler initially.
//
g_pfnTSHandler = 0;
//
// Enable the peripherals used by the touch screen interface.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
SysCtlPeripheralEnable(TS_P_PERIPH);
SysCtlPeripheralEnable(TS_N_PERIPH);
SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER1);
//
// Configure the ADC sample sequence used to read the touch screen reading.
//
ADCHardwareOversampleConfigure(ADC0_BASE, 4);
ADCSequenceConfigure(ADC0_BASE, 3, ADC_TRIGGER_TIMER, 0);
ADCSequenceStepConfigure(ADC0_BASE, 3, 0,
ADC_CTL_CH_YP | ADC_CTL_END | ADC_CTL_IE);
ADCSequenceEnable(ADC0_BASE, 3);
//
// Enable the ADC sample sequence interrupt.
//
ADCIntEnable(ADC0_BASE, 3);
IntEnable(INT_ADC3);
//
// Configure the GPIOs used to drive the touch screen layers.
//
GPIOPinTypeGPIOOutput(TS_P_BASE, TS_XP_PIN | TS_YP_PIN);
GPIOPinTypeGPIOOutput(TS_N_BASE, TS_XN_PIN | TS_YN_PIN);
GPIOPinWrite(TS_P_BASE, TS_XP_PIN | TS_YP_PIN, 0x00);
GPIOPinWrite(TS_N_BASE, TS_XN_PIN | TS_YN_PIN, 0x00);
//
// See if the ADC trigger timer has been configured, and configure it only
// if it has not been configured yet.
//
if((HWREG(TIMER1_BASE + TIMER_O_CTL) & TIMER_CTL_TAEN) == 0)
{
//
// Configure the timer to trigger the sampling of the touch screen
// every millisecond.
//
TimerConfigure(TIMER1_BASE, (TIMER_CFG_16_BIT_PAIR |
TIMER_CFG_A_PERIODIC |
TIMER_CFG_B_PERIODIC));
TimerLoadSet(TIMER1_BASE, TIMER_A, (SysCtlClockGet() / 1000) - 1);
TimerControlTrigger(TIMER1_BASE, TIMER_A, true);
//
// Enable the timer. At this point, the touch screen state machine
// will sample and run once per millisecond.
//
TimerEnable(TIMER1_BASE, TIMER_A);
}
}
//*****************************************************************************
//
//! Sets the callback function for touch screen events.
//!
//! \param pfnCallback is a pointer to the function to be called when touch
//! screen events occur.
//!
//! This function sets the address of the function to be called when touch
//! screen events occur. The events that are recognized are the screen being
//! touched (``pen down''), the touch position moving while the screen is
//! touched (``pen move''), and the screen no longer being touched (``pen
//! up'').
//!
//! \return None.
//
//*****************************************************************************
void
TouchScreenCallbackSet(long (*pfnCallback)(unsigned long ulMessage, long lX,
long lY))
{
//
// Save the pointer to the callback function.
//
g_pfnTSHandler = pfnCallback;
}
//*****************************************************************************
//
// Close the Doxygen group.
//! @}
//
//*****************************************************************************
HELLO WIDGET.C程序:
#include "inc/hw_types.h"
#include "driverlib/interrupt.h"
#include "driverlib/sysctl.h"
#include "grlib/grlib.h"
#include "grlib/widget.h"
#include "grlib/canvas.h"
#include "grlib/pushbutton.h"
#include "drivers/kitronix320x240x16_ssd2119_8bit.h"
#include "drivers/touch.h"
#include "drivers/set_pinout.h"
//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>Hello using Widgets (hello_widget)</h1>
//!
//! A very simple ``hello world'' example written using the Stellaris Graphics
//! Library widgets. It displays a button which, when pressed, toggles
//! display of the words ``Hello World!'' on the screen. This may be used as
//! a starting point for more complex widget-based applications.
//
//*****************************************************************************
//*****************************************************************************
//
// Forward reference to various widget structures.
//
//*****************************************************************************
extern tCanvasWidget g_sBackground;
extern tPushButtonWidget g_sPushBtn;
//*****************************************************************************
//
// Forward reference to the button press handler.
//
//*****************************************************************************
void OnButtonPress(tWidget *pWidget);
//*****************************************************************************
//
// The heading containing the application title.
//
//*****************************************************************************
Canvas(g_sHeading, &g_sBackground, 0, &g_sPushBtn,
&g_sKitronix320x240x16_SSD2119, 0, 0, 320, 23,
(CANVAS_STYLE_FILL | CANVAS_STYLE_OUTLINE | CANVAS_STYLE_TEXT),
ClrDarkBlue, ClrWhite, ClrWhite, &g_sFontCm20, "hello-widget", 0, 0);
//*****************************************************************************
//
// The canvas widget acting as the background to the display.
//
//*****************************************************************************
Canvas(g_sBackground, WIDGET_ROOT, 0, &g_sHeading,
&g_sKitronix320x240x16_SSD2119, 0, 23, 320, (240 - 23),
CANVAS_STYLE_FILL, ClrBlack, 0, 0, 0, 0, 0, 0);
//*****************************************************************************
//
// The button used to hide or display the "Hello World" message.
//
//*****************************************************************************
RectangularButton(g_sPushBtn, &g_sHeading, 0, 0,
&g_sKitronix320x240x16_SSD2119, 60, 60, 200, 40,
(PB_STYLE_OUTLINE | PB_STYLE_TEXT_OPAQUE | PB_STYLE_TEXT |
PB_STYLE_FILL | PB_STYLE_RELEASE_NOTIFY),
ClrDarkBlue, ClrBlue, ClrWhite, ClrWhite,
&g_sFontCmss22b, "Show Welcome", 0, 0, 0, 0, OnButtonPress);
//*****************************************************************************
//
// The canvas widget used to display the "Hello!" string. Note that this
// is NOT hooked into the active widget tree (by making it a child of the
// g_sPushBtn widget above) yet since we do not want the widget to be displayed
// until the button is pressed.
//
//*****************************************************************************
Canvas(g_sHello, &g_sPushBtn, 0, 0,
&g_sKitronix320x240x16_SSD2119, 0, 150, 320, 40,
(CANVAS_STYLE_FILL | CANVAS_STYLE_TEXT),
ClrBlack, 0, ClrWhite, &g_sFontCm40, "Hello World!", 0, 0);
//*****************************************************************************
//
// A global we use to keep track of whether or not the "Hello" widget is
// currently visible.
//
//*****************************************************************************
tBoolean g_bHelloVisible = false;
//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, unsigned long ulLine)
{
}
#endif
//*****************************************************************************
//
// This function is called by the graphics library widget manager in the
// context of WidgetMessageQueueProcess whenever the user releases the
// "Press Me!" button. We use this notification to display or hide the
// "Hello!" widget.
//
// This is actually a rather inefficient way to accomplish this but it's
// a good example of how to add and remove widgets dynamically. In
// normal circumstances, you would likely leave the g_sHello widget
// linked into the tree and merely add or remove the text by changing
// its style then repainting.
//
// If using this dynamic add/remove strategy, another useful optimization
// is to use a black canvas widget that covers the same area of the screen
// as the widgets that you will be adding and removing. If this is the used
// as the point in the tree where the subtree is added or removed, you can
// repaint just the desired area by repainting the black canvas rather than
// repainting the whole tree.
//
//*****************************************************************************
void
OnButtonPress(tWidget *pWidget)
{
g_bHelloVisible = !g_bHelloVisible;
if(g_bHelloVisible)
{
//
// Add the Hello widget to the tree as a child of the push
// button. We could add it elsewhere but this seems as good a
// place as any. It also means we can repaint from g_sPushBtn and
// this will paint both the button and the welcome message.
//
WidgetAdd((tWidget *)&g_sPushBtn, (tWidget *)&g_sHello);
//
// Change the button text to indicate the new function.
//
PushButtonTextSet(&g_sPushBtn, "Hide Welcome");
//
// Repaint the pushbutton and all widgets beneath it (in this case,
// the welcome message).
//
WidgetPaint((tWidget *)&g_sPushBtn);
}
else
{
//
// Remove the Hello widget from the tree.
//
WidgetRemove((tWidget *)&g_sHello);
//
// Change the button text to indicate the new function.
//
PushButtonTextSet(&g_sPushBtn, "Show Welcome");
//
// Repaint the widget tree to remove the Hello widget from the
// display. This is rather inefficient but saves having to use
// additional widgets to overpaint the area of the Hello text (since
// disabling a widget does not automatically erase whatever it
// previously displayed on the screen).
//
WidgetPaint(WIDGET_ROOT);
}
}
//*****************************************************************************
//
// Print "Hello World!" to the display on the Intelligent Display Module.
//
//*****************************************************************************
int
main(void)
{
//
// Set the system clock to run at 50MHz from the PLL
//
SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_16MHZ);
//
// Set the device pinout appropriately for this board.
//
PinoutSet();
//
// Enable Interrupts
//
IntMasterEnable();
//
// Initialize the display driver.
//
Kitronix320x240x16_SSD2119Init();
//
// Initialize the touch screen driver.
//
TouchScreenInit();
//
// Set the touch screen event handler.
//
TouchScreenCallbackSet(WidgetPointerMessage);
//
// Add the compile-time defined widgets to the widget tree.
//
WidgetAdd(WIDGET_ROOT, (tWidget *)&g_sBackground);
//
// Paint the widget tree to make sure they all appear on the display.
//
WidgetPaint(WIDGET_ROOT);
//
// Loop forever, processing widget messages.
//
while(1)
{
//
// Process any messages from or for the widgets.
//
WidgetMessageQueueProcess();
}
}