This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

为什么TPS5430效率只有50%左右?

Other Parts Discussed in Thread: TPS5430

你好,我现在用了一颗TPS5430,24V转5V给我设备供电,测的效率很低只有50%左右,电路图如下,TPS5430输入端:26.26V  22mA,TPS5430输出端:4.84V 67mA,效率只有56.13%。

电路图看附件。