This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM3168A: PCM3168AEVM Rev A 自启动程序测试问题点 用PPC3写入I2C无输出

Part Number: PCM3168A

尊敬的TI

遇到以下问题,咨询如何解决方案

问题1:PCM3168AEVM Rev A评价板自启动程序,IN5/IN6差分模拟输入,OUT7/OUT8均有输出且输出相当,但是OUT7的残留噪声是OUT8的5倍,OUT7残留噪声:109.3μV,OUT8残留噪声:24.63μV,请问问题出在哪儿?

问题2:利用PPC3软件写入I2C寄存器,在基板I2C测试点进行测量,显示PCM3168寄存器已经写入,并有低电平的ACK,IN5/IN6差分模拟输入,OUT输出端口就是没有输出,请问原因在哪儿?能提供IN5/IN6差分模拟输入,OUT7/OUT8差分模拟输出的启动条件及软件吗?

  • 您好,收到了您的案例,调查需要些时间,感您的耐心等待。

  • 问题1:两个通道的输入信号是否相同?即使芯片断电,残余噪声差异是否仍然存在?最好检查噪声是否确实来自等效矢量幅度(EVM),而不是由于测量差异。两者的性能应非常接近。
    问题2:如果您使用的是通过电子邮件提供给Alpine的快速入门PowerPoint,那么这就是唯一需要的软件。其中包含了脚本示例。如果您使用的是不同的寄存器配置,请提供给我们以便我们进行复核。此外,设置也很重要:在向板卡写入任何内容之前,请确保SYSCLOCK和电源均已就绪。