This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1502A的XSMT Pin (Soft Mute / Soft Un-Mute)硬件连接问题

Other Parts Discussed in Thread: PCM5102A

Dear Sir,

   我们准备使用PCM1502A进行I2S to Analog 转换,datasheet中XSMT PIN的硬件用法有几个地方存在歧义。

 现在DVDD准备使用1.8V,即数字IO口(I2S)为1.8V。不准备使用DAC的MUTE功能,按理应该上拉到DVDD电源?但是datasheet中写Un-MUTE 数字部分需要大于2V(11.3中),或者直接连接到AVDD(9.3.3)?但是看11.2.2应该是IC内部有默认上拉的,应该悬空就是默认Un-MUTE。到底哪个是对的?谢谢!

11.3


9.3.3中:

11.2.2:

  • 是PCM1502吗,我好像没看到手册,DVDD支持1.8V供电对吧。

  • 产品型号是PCM5102A? 对吧?

    DVDD是1.8V, 不用soft mute, 正确解法就是连到DVDD

     实际上,DVDD用1.8V, soft mute 不再工作(也无法工作),1.8V un-mute设备。 XSMT to 0V , hard mute 设备。

  • 是的,型号是PCM5102A。

    datasheet中没有写1.8V  soft  mute是无效状态,现在担心的是XSMT连接到1.8V(DVDD)将会soft mute,这样就会一直处于mute状态,没有模拟输出了。

    代理商说连接到不用时连接到AVDD,不到2V会mute,但是这个写的是DVDD是3.3V的连接方式。

    看datasheet中的框图,不用时是可以不连接的,因为框图用了一个二极管反向到控制端,这就说明应该是IC内部上拉了。但是datasheet中又没有写。所以就纠结了。。我现在的设计是兼容了3.3V和1.8V两种上拉。。

  • 是PCM1502A,PCM1502已经不推荐在新设计中使用了。DVDD支持1.8V。

  • 确认1.8V, soft mute 无效。XSMT 输入范围-0.3 to DVDD+0.3. 并需要接高 才会soft mute 无效。

  • 好的。建议更新下datasheet,不然会导致歧义。谢谢!

  • 您好!我们新设计中准备使用PCM5102A芯片,但是数据手册中对于智能静噪功能的描述和配置比较模糊。手册中介绍可实现112dB的动态调节范围具体指示是哪方面?

    期待您的回复!