This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助:PCM1794两声道输出相差1dB

Other Parts Discussed in Thread: PCM1794A

一张1794的DAC板子,CS8422 I2S到PCM1794A,左右两声道输出相差1dB。已经检查过IV和LPF电路正常,金属膜电阻和NPO电容都老化稳定后,电桥在50hZ、1KHZ\10KHZ挑过,数值相差很小0.5%以内。两声道的相差从IV输出开始就有10%左右的电平差别。尝试更换左右输出声道的运放,但是没有变化。甚至尝试更换1794a,问题依旧。因此求助各位。谢谢!以往做过的多种DAC两声道差异都在0.1dB以内。

  • 既然换了运放, 换了 PCM1794A 问题依旧, 那么还有板上器件的问题, 以及信号源或设置问题.

    因为 DAC 的输出驱动能力都不强, 所以外围器件的影响也很有可能, 值得检查一下

  • 可以用示波器观察一下中间节点的信号,比如I/V转换级电压是否一样,输出端差动放大器节点电压是否一致。可能电阻的问题比较大,包括电阻的焊接发热等。

  • 因为工作外派很久不来了,不知道1794A的输出阻抗阁下有无了解。也想起一个细节,1794A信号小的一声道,IC的PCB焊盘和输出线路不小心被弄断了,之后我自己小飞线接上的。测量到IV级运放PIN脚处的直流电阻与另一正常声道比大0.08欧,不知道这一点有无影响。记忆中一些TI老DAC片子标称的输出阻抗都在2/300欧的状态,但可惜的是1794A没有标准这个参数。如果1794A的输出内阻在100以上,按理说是0.1欧的差异不会有什么影响。

  • 从DAC片子出来到I/V转级、再到LPF、缓冲各级运的供电电压是一致的。但是从IV输出开始的波形幅度就有差异了,同时示波器直接量1794A输出信号量不到,不知道是不是探头不是差分的,或者是示波器灵敏度不够。现在比较疑惑1794A的输出等效阻抗,可惜DATASHEET上找不到。我的板子左声道输出线弄断了自己短飞线接上了。飞线很短5mm左右的镀银细铜线,比正常一声道到IV运放PIN脚端的直流电阻大0.08欧姆。去掉IV运放测量各电阻的值两声道差异很小,还是0.5%以内。

  • I/V转换输出就有误差,那么只有两点,一点事I/V转换的反馈电阻不匹配,可以拆下来量一下。第二个是DAC到I/V转换运放的距离要匹配,因为这个阻抗会影响有效信号和I/V的倍数。