This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

两颗TAS5711,一颗作2.0输出,一颗作PBTL输出,共用一个I2S_DATA时发现失真增大,TI的demo板输出36W(DC24V供电)只有1%失真。但我这个组合却为3%。如何解决这个问题?

Other Parts Discussed in Thread: TAS5711

TI的工程专家们:

   你们晚上好,请指导解决一个问题:

问题描述:

两颗TAS5711,一颗设置为2.0输出:16W*2CH,一颗设置为PBTL输出:36W*1CH,共用一个I2S_DATA。

测试结果:

1.PBTL:36W(24Vdc供电),失真3%。

2.BTL:16W*2CH(24Vdc供电 ,失真1.5%。

3.测试TI demo 板:PBTL36W失真1%,BTL16W*2CH失真0.7%。

4.把I2S_DATA断开,只连接一个PBTL的IC,测试失真为2%。

请教如何解决上述问题。(附上原理图)

tas5711X2.pdf