This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3101接数字MIC增益小且带直流分量问题



@TI engineer:

本公司有一项目采用4个ADC3101进行8路数字MIC语音采集,并通过IIS将8路语音数据传输给MCU,

16K采样率,16位采样位数,

通过PLL,NADC,MADC配置ADC_MOD_CLK=1.28M

DMCLK output = ADC_MOD_CLK output for the digital microphone

目前功能都调OK,唯一还有如下二个问题来这里咨询下:

1、出来语音数据带有-3000左右的直流分量;

2、增益偏小,Page0 REG83&REG84设置到最大增益20dB也还是偏小

奇怪的是,在增益设置不变的情况下,调大送给数字MIC的CLK频率,实际的增益就会变大,同时直流分量也变得更大。

调来调去,ADC3101 datasheet有关数字MIC的部门看了好几遍,该设置的,能设置的都试了,还是找不到原因,

而数字MIC的PDM只要adc3101给出一个DCLK也没别的可以设置的,

请指教!