TI大神,求助,
我想将3204配置成两路同时输出音频,应该怎样配置寄存器呢
我尝试配置为:
Page1:
"0001", "0C08", "0D08", "0E08",
"0F08", "093C", "1000", "1100",
"1200", "1300", "0000",
主要配置了这些,但是还是只有HPL有声音,LOL没有。
是哪儿不对么
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你的意思是想差分,HPL,HPR输出,同时LOL,LOR也输出是吗?那LOL没输出,看下寄存器Page0, reg37是否将其power down了?
是这样的:
我单独内置或者外置放音都没问题,现在需要两个同时输出;
单独hpl放音寄存器:"0001", "0C08", "0D08", "0930", "1000", "1100", "0000",有声
单独lineout:"0001", "0E08", "0F08", "090C", "1200", "1300", "0000",有声
然后我配置两者同时放音:"0001", "0C08", "0D08", "0E08", "0F08", "093C", "1000", "1100", "1200", "1300", "0000",HPL有声,LOL无声。
却只有hpl有声音。我尝试p0-reg37设置为0xE0,也没效果。还有什么地方需要注意的呢