This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM3070怎么设置LOL和LOR都是一样的输出

Other Parts Discussed in Thread: PCM3070

现在设置的是LDAC输出到LOL(PAGE 1 REG14 D3=1), RADC输出到LOR(PAGE 1 REG15 D3=1).

I2S把两个声道混音,即两个声道输入一样的声音的时候,单个声道输出大小正常,两个声道同时输出的时候几乎听不到声音了,猜测是两个声道一样的声音,一个正,一个负,抵消了。

想把PCM3070设置成两个声道都是一样的输出,试了很久,怎么配置,都不成功。请教如何配置才能实现?

  • 没有声音的时候,用示波器看LOL和LOR的输出波形了吗?
    另外,LOL/LOR Driver Gain有没有设置呢?
  • 用示波器的两个通道,同时看LOL和LOR,每一个都有,但是同相位的地方看到电位是反的,比如LOL上升的时候,LOR是下降的,目前现象是,接LOL或者LOR其中一个到功放,声音大小正常的,两个同时接入功放的左右声道,几乎听不到声音。

    LOL/LOR Driver Gain设置的都是0dB

  • 我的使用目的:MAL和MAR直接输出到HPL和HPR,不经过ADC和DAC,可行。I2S输入的信号(左右声道数据送出来一样的数据)给到DAC之后从LOL和LOR输出,分别接功放的左右声道输出。page 1 寄存器12,13,14,15是设置路径的,值分别为:
    02(MAL output is routed to HPL)
    02(MAR output is routed to HPR)
    08(Left Channel DAC reconstruction filter output is routed to LOL)
    08(Right Channel DAC reconstruction filter output is routed to LOR)
    最后效果就是:接LOL或者LOR其中一个到功放,声音大小正常的,两个同时接入功放的左右声道,几乎听不到声音。不知道是否哪里还需要设置或者哪里设置不对?