This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 EVM 音频采集噪声问题

Other Parts Discussed in Thread: TLV320AIC3106

大家好!我现在是在用DM8168 evm做音频实时采集并回放的测试,现在遇到一个音频采集出现噪声的问题。

环境:

1、平台:DM816x/C6A816x/AM389x EVM

2、sdk:DVRRDK_03.00.01.03

3、OS定制版本:Linux dm816x  2.6.37

4、音频芯片:     tlv320aic3106

5.   测试连接:

音频采集通道:mp3普通耳机输出口->3.5mm转3.5mm数据线->DM8168 EVM的Line in音频输入口

音频回放通道: HP out->普通耳机

问题描述:

在做音频采集并实时回放的测试时,可以正常采集并实时回放,但是有非常明显的噪声,MP3播放器的音量调大时,噪声更加明显,但是音频素材的音调和内容是完整的,没有数据丢失,感觉是叠加了一层背景噪声。音量调小时,噪声也明显变小。

我把音源换成PC的音频输出(前喇叭输出),存在同样的问题。

请教一下大家这种问题是怎么原因造成的?