Other Parts Discussed in Thread: TLV320AIC23B
最近的项目想用到TLV320AIC23B音频编解码器,具体用法是这样的:
1、一路MIC信号通过运放放大并反向成2路差分信号给AIC23B的线路输入端LLINEIN和RLINEIN;
2、AIC23B线路输出LINEOUT通过外部运放放大后给600Ω阻抗耳机;
3、I2S和I2C接控制芯片;
有以下几个问题想确认:
1、HPVDD需要接吗?;
2、2-WIRE模式是指I2C吗?看了以下时序,应该是满足I2C的,但是这里为什么叫2-WIRE模式呢?
3、I2C只能写不能读吗?
4、线路输出可以这样接运放吗,一般运放输入阻抗比较大,能否驱动?
5、第2章的特性参数表中的数据是在DVDD=1.5V的情况下的,如果用3.3V电压,参数会有变化吗?