Other Parts Discussed in Thread: CC8530, CC2590, LM49350
1、看AIC3254的手册,他有secondary I2S,是不是说有两套I2S接口?可以有两个DIN,两个DOUT,我现在有两个话筒,每个话筒各有左右声道输入,也就是共有4个通道的语音输入,是否可以?
2、CC8530的I2S AD0,AD1可配置为输入输出,准备将AD0,AD1设置为输出,分别接两路3254的两路I2S的DIN,是否可行?
3、原理图中CC2590的AVDD_BIAS,AVDD_LNA,AVDD_PA分别接了一个电感,这个电感是器件还是PCB走线?
4、音量增减和开关机按键,是高有效还是低有效?为什么开关机按键接到CSN,长时间按住会开关CC8530,即使power ON/OFF,也只是控制了CC8530,其他芯片还在工作,这个是不是真正意义的开关机
5、3254能否接受4个通道的语音,通过混音后输出?