This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教下swrr079压缩包中CC85XX headset reference design 1_3_SCHEMATIC原理图中几个问题(AIC3254,CC8530)

Other Parts Discussed in Thread: CC8530, CC2590, LM49350

1、看AIC3254的手册,他有secondary I2S,是不是说有两套I2S接口?可以有两个DIN,两个DOUT,我现在有两个话筒,每个话筒各有左右声道输入,也就是共有4个通道的语音输入,是否可以?

2、CC8530的I2S AD0,AD1可配置为输入输出,准备将AD0,AD1设置为输出,分别接两路3254的两路I2S的DIN,是否可行?

3、原理图中CC2590的AVDD_BIAS,AVDD_LNA,AVDD_PA分别接了一个电感,这个电感是器件还是PCB走线?

4、音量增减和开关机按键,是高有效还是低有效?为什么开关机按键接到CSN,长时间按住会开关CC8530,即使power ON/OFF,也只是控制了CC8530,其他芯片还在工作,这个是不是真正意义的开关机

5、3254能否接受4个通道的语音,通过混音后输出?

 

  • 1. 两个I2S是内部开关切换的,不能同时使用。AIC3254内部是立体声,没有真正的四声道。

    5. 可以通过左右模拟+左右I2S接受4CH,但是我想和你的需求不一致。

  • 感谢Ryan的回复!

    能否帮助推荐一个两个I2S的音频Codec,且带MiniDSP,做一些降噪,3D等音效处理。

    我们在TI网站上没有找到。如果没有,我们考虑采用2个AIC3254芯片实现4个声道,2个I2S。但其他几个问题仍然困扰着我们:

    原理图中CC2590的AVDD_BIAS,AVDD_LNA,AVDD_PA分别接了一个电感,这个电感是器件还是PCB走线?

    4、音量增减和开关机按键,是高有效还是低有效?为什么开关机按键接到CSN,长时间按住会开关CC8530,即使power ON/OFF,也只是控制了CC8530,其他芯片还在工作,这个是不是真正意义的开关机

    5、3254能否接受4个通道的语音,通过混音后输出?

    麻烦帮助。

    谢谢!

  • 您好,

    TI的LM49350是2个I2S的音频codec,不带有miniDSP;AIC3262是3路I2S的codec,内置miniDSP。

    问题2,3,4可以到"技术论坛-无线连接"里咨询查证。

    5,如果是4路模拟音源,支持模拟前端混音,但是做codec以及内部dsp处理时只能是2路。