This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tlv320aic32x4芯片播放模式时,用示波器i2s接口上有波形信号,HPL上没有波形输出

mclk为12.288MHz,

用adb执行如下命令播放48K_16bit_stereo.wav时,寄存器配置如下log:

tinymix "QUAT_MI2S_RX Audio Mixer MultiMedia1" "1"
tinymix "HPL Output Mixer L_DAC Switch" "1"
tinymix "HP DAC Playback Switch" "1"
tinyplay /sdcard/48K_16bit_stereo.wav

log:

[aic32x4] aic32x4_write page =  1, reg =    c(012), val =    8    //Left Channel DAC reconstruction filter's positive terminal is routed to HPL

[aic32x4] aic32x4_write page =  1, reg =  10(016), val =    0    //HPL driver gain is 0dB
[aic32x4] aic32x4_write page =  1, reg =  11(017), val =    0    //HPR driver gain is 0dB

[aic32x4] aic32x4_write page =  0, reg =  40(064), val =   12   //Left DAC Channel muted,Right DAC Channel muted

[aic32x4] aic32x4_write page =  0, reg =    4(004), val =    3    //PLL Clock is CODEC_CLKIN
[aic32x4] aic32x4_write page =  0, reg =  1d(029), val =    1    //BDIV_CLKIN = DAC_MOD_CLK
[aic32x4] aic32x4_write page =  0, reg =    5(005), val =   17   //PLL divider P Value 1,PLL divider R Value 1
[aic32x4] aic32x4_write page =  0, reg =    6(006), val =    8    //PLL divider J value 8
[aic32x4] aic32x4_write page =  0, reg =    7(007), val =    7    //PLL divider D value (MSB) 7
[aic32x4] aic32x4_write page =  0, reg =    8(008), val =  128  //PLL divider D value (LSB) 128
[aic32x4] aic32x4_write page =  0, reg =    b(011), val =    2    //NDAC Value 2
[aic32x4] aic32x4_write page =  0, reg =    c(012), val =    8    //MDAC Value 8
[aic32x4] aic32x4_write page =  0, reg =    d(013), val =    0    //DAC OSR (DOSR) Setting MSB
[aic32x4] aic32x4_write page =  0, reg =    e(014), val =  128  //DAC OSR (DOSR) Setting LSB 128
[aic32x4] aic32x4_write page =  0, reg =  12(018), val =    2    //NADC Value 2
[aic32x4] aic32x4_write page =  0, reg =  13(019), val =    8    //MADC Value 8
[aic32x4] aic32x4_write page =  0, reg =  14(020), val =  128  //128(Use with PRB_R1 to PRB_R6, ADC Filter Type A)
[aic32x4] aic32x4_write page =  0, reg =  1e(030), val =    4    //BCLK N Divider value 4
[aic32x4] aic32x4_write page =  0, reg =  1b(027), val =    0    //Audio Interface = I2S  Data Word length = 16 bits BCLK is input to the device WCLK is input to the
[aic32x4] aic32x4_write page =  0, reg =   3f(063), val =  148  //Left DAC Channel Powered Up,Left DAC data Left Channel Audio Interface Data,Soft-Stepping is 1
[aic32x4] aic32x4_write page =  1, reg =    9(009), val =   32   //HPL is powered up
[aic32x4] aic32x4_write page =  0, reg =    5(005), val =  145  //PLL is powered up,PLL divider P Value 1,PLL divider R Value 1
[aic32x4] aic32x4_write page =  0, reg =    b(011), val =  130  //NDAC divider powered up,NDAC Value 2
[aic32x4] aic32x4_write page =  0, reg =    c(012), val =  136  //MDAC divider powered up,MDAC Value 8
[aic32x4] aic32x4_write page =  0, reg =  12(018), val =  130  //NADC divider powered up,NADC Value 2
[aic32x4] aic32x4_write page =  0, reg =  13(019), val =  136  //MADC divider powered up,MADC Value 8
[aic32x4] aic32x4_write page =  0, reg =  1e(030), val =  132  //BCLK N divider powered up,BCLK N Divider value 4
[aic32x4] aic32x4_write page =  0, reg =  40(064), val =    0    //Left and Right Channel have independent volume control, not muted

  • 开机过程aic32x4_probe时增加配置电源后解决,
    [aic32x4] aic32x4_write page = 1, reg = 2(002), val = 9( 9) //Power up AVDD LDO
    [aic32x4] aic32x4_write page = 1, reg = 1(001), val = 8( 8) //Disable weak AVDD in presence of externa AVDD supply
    [aic32x4] aic32x4_write page = 1, reg = 2(002), val = 1( 1) //Enable Master Analog Power Contro,Power up AVDD LDO