Other Parts Discussed in Thread: TAS2505
Hi TI TAS2505 專家,
想請問一下, TAS2505 正常操作下, IC 各個 power rail 所吃的電流數據
I(AVDD), I(DVDD), I(IOVDD), I(SPKVDD)
datasheet 裡只有 shutdown 時的電流
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Amy,
感謝你的回復,
是這樣的
我去看了手冊中的2.5章節, 看到的是下圖, isVDD, IAVDD, IDVDD, iIOVDD 都是mW 等級的
但我們的datasheet 中Electrical Characteristics (continued) 裡的 Po Maximum output power 顯示的是 可以support 從0.8W 到2W
我的客戶是想預估, 提供給TAS2505各個 power rail 到底需要多少的電流才夠
例如 datasheet 所說的2W , 當SPKVDD= 5.5V 時 , 2W/5.5V = 0.36A
也就是說, 設計5.5V 的input power, 我選用的 DCDC converter, 電流要能支持到0.36A
Datasheet