This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS2505输出失真

Other Parts Discussed in Thread: TAS2505

用TAS2505IR驱动车规级蜂鸣器,增益设置为:

一级放大

-18dB

二级放大

0dB

三级放大

24dB

输入输入1KHz 0dB 单声道 WAV格式的正弦波信号,蜂鸣器两端的波形失真(被切削,且变成了5KHz,反复折叠?);把“1KHz 0dB 单声道 WAV格式的正弦波信号”这个音源信号衰减7dB,蜂鸣器两端的波形是1KHz的方波。

问题如下:

问题1、从输出波形上来看,0dB的信号被折叠(?)了,这是什么原因?是在哪个阶段产生的?

问题2、输入I2S格式的音频信号,信号幅度有什么限制?

  • 您好,

    我不太确定TAS2505是否可以驱动蜂鸣器,可以附一下蜂鸣器的规格书吗
  • 见附件,是扬声器,不是蜂鸣器8726.BMS3408-01 LF.pdf

  • 有可能是总的增益设置太大了,导致输出信号失真,您有没有尝试将TAS2505的SPK增益或DAC增益设置小一些看信号输出效果呢
  • 如附件的音源文件,无论怎么调整DAC增益都会失真。

    如果将音频文件衰减9dB,DAC增益按如下设置,Speaker两端就是类似于方波的波形:

    一级放大  -12
    二级放大  0
    三级放大  24

     

    以前客户说仪表报警声音量小,失真严重,现在把Speaker更换成附件中Speaker,音量达到了客户的要求,客户又说报警声音色不理想,需要如何设置寄存器?BDT38.5-11B-08H20-BOX.pdfBDT38.5-11B-08H20-BOX.pdf