This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA6120A2平衡输出功率问题

Other Parts Discussed in Thread: TPA6120A2, OPA1642

Dears:

  我们在测试应用TPA6120大电流运放,做一个平衡输出电路。如下面截图,这是我们之前一个单端输出的项目,输出接32Ω负载对地,功率可以做到1.5W。

    但输入平衡信号,输出采用桥接的方式做平衡输出带负载,功率就达不到1W,并且TPA6120温度上升很快,输出5.7Vrms时,仅能大约工作几分钟就会在TPA6120输出端出现直流。

    请帮忙看下这种接法是有什么问题吗?

    (此平衡接法电路我们应用很普遍,但是还未做过很大的功率,此次应用TPA6120主要是考虑输出功率,目标是做到1.5W~2W)

  • 您好,
    LAGND、RAGND、AGND是接在一起的吗,是-12V和+12V中间电压吗,还有R1接的也是LAGND吗
    R7和R33的作用是什么
    不太明白您为什么使用两个运放,您把TPA6120A2用作了电压跟随器,如果您需要TPA6120A2的驱动能力,您可以将TPA6120A2接成OPA1642的形式,OPA1642就可以省去
    关于TPA6120输出端出现直流,您有同时测量输入信号吗,输出直流时,输入信号是怎样的,输出直流幅值是多少
  • LAGND/RAGND/AGND是接到一起的,单点接地。±12V是相对于AGND的电压。R1接到了AGND。

    两个运放是前级1642做电压放大,后级仅仅作为电流放大。如果只用TPA6120A2做放大电路,将会有较高的噪声。