This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC3100: Is the official website driver available?

Part Number: TLV320ADC3100

Our company uses this IC for recording. We downloaded the driver from the official website, and the register configuration is as follows, but the recording failed. Is there a problem with register configuration?

[root@newx:/]# i2cdump -f -y 1 0x18
No size specified (using byte-data access)
     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f    0123456789abcdef
00: 00 00 20 00 00 11 18 00 00 00 00 00 00 00 00 00    .. ..??.........
10: 00 00 90 86 40 80 04 00 00 00 01 0c 00 03 81 00    ..??@??...??.??.
20: 00 10 00 00 00 00 02 00 00 00 00 00 00 00 00 00    .?....?.........
30: 00 00 00 28 04 12 02 02 00 00 00 44 00 01 00 00    ...(????...D.?..
40: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
50: 00 00 88 00 00 00 00 00 7f 00 00 00 00 00 00 00    ..?.....?.......
60: 7f 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ?...............
70: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
90: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................