Part Number: TLV320ADC3100
Our company uses this IC for recording. We downloaded the driver from the official website, and the register configuration is as follows, but the recording failed. Is there a problem with register configuration?
[root@newx:/]# i2cdump -f -y 1 0x18
No size specified (using byte-data access)
0 1 2 3 4 5 6 7 8 9 a b c d e f 0123456789abcdef
00: 00 00 20 00 00 11 18 00 00 00 00 00 00 00 00 00 .. ..??.........
10: 00 00 90 86 40 80 04 00 00 00 01 0c 00 03 81 00 ..??@??...??.??.
20: 00 10 00 00 00 00 02 00 00 00 00 00 00 00 00 00 .?....?.........
30: 00 00 00 28 04 12 02 02 00 00 00 44 00 01 00 00 ...(????...D.?..
40: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
50: 00 00 88 00 00 00 00 00 7f 00 00 00 00 00 00 00 ..?.....?.......
60: 7f 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ?...............
70: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
90: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................