This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
通过Mouser采购一批NE5532运放,官网显示封装为SO-8,收货时发现为宽体封装,和通用SO-8或SOIC-8差别较大,不能兼容贴片。回头检查了一下规格书,发现芯片的SOP-8两边焊脚间距为7mm左右,正常SO-8应为5.2mm左右,再去Mouser官网看了一下可供下载的AD库文件,也是5.2mm左右正常SO-8库文件,不知道责任如何界定?Mouser要求再TI官网发帖,由Ti工程师进行鉴定,好像是这个意思。
Mouser SOP-8的3D库文件左右间距到是7.2mm无误,如果购买前能下载一下这个文件到是可以发现问题。下面是Mouser NE5532PSR产品链接
您好,您购买的NE5532的完整型号是什么?如果是SO-8的封装,型号应该为NE5532PSR.
如果您购买的是SOIC-8的封装, 那么完整的型号应该为NE5532D,NE5532DR或者NE5532DRG4.
所以根据型号,就能判断您具体买的是5.2mm的SO-8封装还是7mm的SOIC-8的封装.
您好,NE5532的datasheet中, SO-8为宽体,SOIC-8 为窄体, 首先您收到的实物是符合datasheet的.
另外,我通过在NE5532的主页上,对应SOIC 8和SO8的供应上,点击Mouser 进去之后,发现Mouser上的规格中封装尺寸也是对应的,SO8 为宽体,SOIC8 为窄体:
https://www.mouser.cn/ProductDetail/Texas-Instruments/NE5532D?qs=7nS3%252BbEUL6sxxFd8wD6aVQ%3D%3D
我又在产品主页的CAD&CAE symbols进去看了下封装库,也是和datasheet中都对应上:
所以现在您的问题是在Mouser上二维封装库显示是对应不上的,对吧? 这个应该和Mouser联系 , 因为目前TI网上的封装信息不管是CAD还是datasheet都是对应的.
另外,我也看了其他型号SO-8 和SOIC-8封装的尺寸,和 NE5532 都是一样的.
比如LM311:www.ti.com/.../LM311