Part Number: TPA3130D2
您好 计划使用TPA3130D2 ,SDZ, MUTE 引脚都 通过MCU进行控制,FAULTZ通过MCU 读取。
1、解决开机POP,是控制SDZ,还是MUTE呢?
2、发生了FAULTZ,TPA3130锁死,怎么让他自恢复呢? 通过MCU怎么控制?
3、FAULTZ 是 开漏输出吗? FAULTZ直接串联10k电阻上拉3.3V 后给MCU可以吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
1、 建议的顺序是上电-----> SDZ low to High----->Mute to Unmute------>Paly audio.
2、FAULTZ拉低的故障有过流、过温和过高的DC Offset,您可以将 FAULTZ pin 连接到 SDZ pin。故障时,FAULTZ 为低电平,shutdown 设备,待故障去除后,FAULTZ 就会高电平,然后设备正常工作;
3、是的,OD输出,可以的,但是建议FAULTZ 与SDZ 连接在一起,这样故障恢复后,可以自动解锁恢复正常工作