多批次(4批次 6k)生产维持在 2%左右不良, 表现为 保护SD脚拉低, 第一脚拉低,更换IC,正常.
请安排工程师联系我
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不知道是不是您的电路发生了DC detect故障,DC detect故障会拉低fault 管脚,并且不能通过SD管脚清除这个故障,只能从新上电PVCC才可以清楚;另外,上电时SD是高电平,也很容易进入DC detect故障,因此,是建议上电时拉低SD,待输入信号稳定后再拉高SD管脚。
看TPA3111D1内部框图,PVCC在输出级连接的是PWM开关电路,如果PVCC的储能电容不够大,我不确定会不会造成DC detect故障,但是肯定会对输出差分电压的占空比产生影响(A DC Detect Fault is issued when the output differential duty-cycle exceeds 14% (for example, 57% or –43%) for more than 420 ms at the same polarity)。因此,建议您上电前拉低SD管脚,待输入稳定后再拉高。同时,PVCC的220uF电容是必须的。
目前,我也不确定您之前测试的故障芯片是不是已经损坏,您可以改善上述2点后,再验证一下;
电路图的其他方面我没看出问题,没有改善的建议。