This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3255: TPA3255测试短路保护时烧功放芯片

Part Number: TPA3255


产品用TPA3255做的功放板,已经做了两年10多批次了,大概有20K左右,之前一直满载输出的时候,短路输出,功放是可以进入短路保护状态的,

  现在这批次,采用36V供电,输出120W的测试短路保护是正常的(PBTL),采用51V供电,输出250W时测试短路保护。大概10块板会烧坏一块板。问供应商也没办法解决,保护电流的电阻也设置30K和64K了,也没能改善。烧了功放芯片后换一个新的功放芯片,测试10多次也不会损坏。请求帮忙分析下,急!!!!