我们TI PCM5101在ASM3M项目上,生产200台,出现了4台关机有明显的POP声音,能够测量出PCM5101的6脚和7脚有波形输出。能否帮忙查看下问题。
原理图部分如下:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
首先,PCM5101 已不推荐用于新设计,请考虑替代产品PCM5101A;
在 PCM5101 datasheet 中 Recommended Powerdown Sequence部分有提到,
在系统设计不充分的情况下,PCM510x在断电时可能会出现一些pop 声。POP是由于设备没有足够的时间来检测电源损耗和启动静音过程而导致的。
PCM510x评估板使用电解去耦电容器避免听到pop声。该电容器在USB或S/PDIF数据丢失和电源丢失之间提供足够的时间,以便静音过程发生。