Part Number: TPA3220EVM
Other Parts Discussed in Thread: TPA3220, TPS3802
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPA3220EVM
Other Parts Discussed in Thread: TPA3220, TPS3802
1、是的,这里手册错误,内部是上拉到了5V,您的测量输出是正确的;这里已确认手册书写错误,但是手册还没有来得及更新。
2、FAULT 故障后,如果故障原因消失后,复位TPA3220可以进入正常工作状态,如果如果故障原因,即使复位TPA3220,还会再次进入FAULT故障状态,表现为FAULT 一直输出低电平,如果短接J13,那么就是一直处于复位状态。解决问题的办法就是找出故障原因,消除掉这个故障原因。FAULT 拉低的原因如下表格截图,因此看下发生故障时,是否出现了过流、过温以及供电电压欠压等:

现在问题是,接入保护电路,TPA3220就不能正常工作,如果断开FAULT引脚,TPA3220就能正常工作,接上之后,下图是自动复位电路,FAULT接TPA3220的PIN4_FAULT脚, RESET接TPA3220的PIN10_RESET脚,只要电路连接FAULT引脚上电,功放就无法正常工作,表现为RESET低电平,CMUTE引脚低电平,FAULT引脚电压在3.8V左右,如果断开FAULT引脚上电,一切正常,只是保护后不会自动复位;我尝试断开FAULT引脚上电后,再连接FAULT,没有问题,但是人为过载保护后,功放芯片就无法正常工作,和连接FAULT上电同样的现象,帮忙分析下问题原因,谢谢

在TPA3220端FAULT管脚您接个上拉看看是否可以解决这个问题?因为TPA3220内部上拉可能太弱,接MR后,可能拉不到高电平,使得FAULT管脚为低电平,进而复位TPA3220
TPS3802K33您是4V供电是吗?您实测供电电压多少?如果供电电压低的话,TPS3802K33也会发出复位信号,如下截图:

如果FAULT引脚电压是3.8V左右的话,对TPS3802K33来说应该是高电平,不会发出复位信号。
您是否已经尝试了在TPA3220的FAULT管脚接上拉?因为我看TPA3220 EVM板也是用的这个TPS3802K33复位芯片,它在FAULT管脚是接上拉的
上拉我一直都有,和TPA3220 EVM一样,47K电阻上拉到5V,这个上拉电阻也尝试改到4.7K,问题依旧,换成4.7K上拉之后,MR可以测量到电压是4.76V,如果断开一下FAULT或者断开一下RESET都能正常,这里是不是有个时序问题?上电之后,FAULT需要上升到5V,但是未达到3.3V之前,芯片是处于复位状态,复位之后,FAULT又有一个上升到5V的过程,周而复始,就一直处于这个复位状态,改变了上拉电阻,FAULT上升的时间快了,虽然我万用表测量的电压是4.76V,但是实际这个是平均值,示波器看应该有瞬时的下拉,所以TPS3802一直处于复位状态?
TPA3220 是有上电时序的,如下手册截图,我不确定您 的FAULT为什么会有瞬时的下拉,如果有瞬时的下拉,那就是不正常的;
您断开FAULT管脚与MR的连接,FAULT管脚输出是一直高电平吗?

我现在断开FAULT与MR的连接,上电,FAULT正常是高电平,RESET高电平,CMUTE高电平,TPA3220正常工作;
这个时候人为过载保护,FAULT输出低电平,RESET仍然高电平,CMUTE仍然高电平,TPA3220无输出,保护状态;
此时FAULT与MR我用短路座连接,FAULT输出高电平,RESET输出低电平,CMUTE输出低电平,TPA3220仍然无输出,然后我拔下短路帽,FAULT高电平,RESET高电平,CMUTE高电平,功放正常输出;
这么测试下来,表明FAULT管脚是正常的,TPS3802K的工作也是正常的,唯一不解的是,一直连接FAULT与MR是不行的,必须要断开一下才能正常复位,麻烦帮忙分析一下,十分感谢!
此时FAULT与MR我用短路座连接,FAULT输出高电平,RESET输出低电平,CMUTE输出低电平,TPA3220仍然无输出,然后我拔下短路帽,FAULT高电平,RESET高电平,CMUTE高电平,功放正常输出;
建议您单独测下(断开与功放的连接)TPS3802K的MR脚,由高变低,再由低变高,看其reset管脚是否可以正常输出?
此时FAULT与MR我用短路座连接,FAULT输出高电平,RESET输出低电平,CMUTE输出低电平,TPA3220仍然无输出,然后我拔下短路帽,FAULT高电平,RESET高电平,CMUTE高电平,功放正常输出;
上述过程建议用示波器同时测量下FAULT和RESET波形,看下FAULT波形是否满足MR的上升速率和下降速率的要求:

电路图我没看出来哪里有问题;
问题的关键点是FAULT和MR脚连接后,FAULT管脚有瞬时的下拉,导致TPS3802一直输出复位信号?您可以附上此时FAULT管脚的波形看下吗