This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5630: TAS5630参数问题

Part Number: TAS5630


应用中希望通过DAC信号驱动TAS5630,TAS5630后接变压器,作为一个可调电源(幅度、频率)。现在有几个问题:

1.

在TAS5630B的数据手册中的描述,圈1的地方,单位为峰峰值,这个是指input A的输入信号吧,如果按双路BTL方式连接,input A与input B做为差分输入,差分值的范围是不是就成了Vpp=10V?

圈2的地方为增益,大约14,是不是对应PVDD_X=50V时,最大输入峰值只需要50/14=3.571V时,输出就达到最大峰值50V?

2.按照TI的单端转差分推荐电路,如果采用TI的OPA320AIDR,强行将DAC输出的Vcom=1.65V,峰值3.3V的信号变作差分,Vp=Vn=(Vcom=2.5V,峰值5V信号)Vp与Vn的共模信号不会绝对相等,是否会有影响?这种输入输出下,有没有超过TAS5630B的输入范围?