Part Number: TPA3255-Q1
带2.5R/600W的功率电阻负载,电流在6-7A左右,TPA3255-Q1的FAULT报警

配置按TPA3255-Q1的PBTL推荐电路设计的

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是哪里的电流从0.5A 一点点增到 7A左右?看您设置的ROCP电阻是27K,OC阈值是14.2A;
根据您描述的过程,应该是先过温,再紧接着过载,过载保护后关断输出,温度不再上升,OTW正常,但还一直处于过载状态中,所以FAULT一直被拉低。
芯片从有输出到没有输出的过程中,供电电压都是正常的吗?