Part Number: TPA3255
我们想用TPA3255,做一款2.1的应用,请问根据M2 M1 INPUT MODE与OUTPUT选择,1*BTL+2*SE,只能是选M2=0,M1=1,这时对应INPUT A,B(OUTPUT BTL),INPUT C,D(C OUTPUT SE,D OUTPUT SE)?请问规格书里的C_START引脚(IN=SE,OUT=BTL),这个IN就是短路帽悬空?OUT就是短路帽连通?请问TPA3255的全中文的规格书有吗?官网的中文说明书只有第一页是中文的,但其它页是英文的。请提供一下中文的规格书,谢谢。TPA3255的GVDD_AB,VDD,GVDD_CD,AVDD,DVDD都接DC12V的话,请问这个DC12V的额定电流大约多少mA的?另外FREQ_ADJ通过30K电阻接地,OC_IOP,OC_IOM引脚分别悬空,这时TPA3255处于MASTER MODE,工作频率是不是450KHZ左右?当处于AM1,AM2模式时工作频率分别是多少KHZ?另外TPA3255上电时序是不是一定要通过TPS3802K33DCKR这颗芯片复位芯片的?上电复位一下后TPA3255才能正常进入工作状态,如果把/RESET引脚悬空不接TPS3802K33DCKR这颗芯片,那TPA3255是没法进入正常工作状态的?



)这个已明白,就是到时有问题,就调整这个C_START引脚的电容大小就好了,没问题就按规格书的参数。/CLIP_OTW,/FAULT指示电路能不能用这样的?不用MOS管
,另外TPA3255这颗芯片是没STBY/MUTE引脚的,到时能不能用MCU的I/O口,把/RESET强行拉低,这样TPA3255就没输出了,来实现MUTE的作用,降低功放的待机功耗。