Other Parts Discussed in Thread: TPA3116D2
使用TPA3118D2做功放,双面板,24V供电,发热严重,几分钟后芯片自动重启,测试芯片表面温度到90多度。输出端接的是200W的大喇叭,现在芯片设成最小的增益(Master 20 dB R1=5.6 kΩR2=OPEN),输入正弦波幅度调到2V时,24V直流稳压源的电流为0.45A左右,TPA3118D2几分钟后直接到90多度,自动重启。如果正弦波幅度调到1V,芯片温度会在80度左右,24V直流电流大概在0.29A。这样算起来总功率都不到10W,芯片就发热严重了,不知道要怎么处理?
,