Part Number: TPA3113D2
Hi, 请教以下TPA3113D2应用问题
1、12V供电,为了兼容2W 8Ω和6W 8Ω喇叭产品设计,当接入2W 8Ω喇叭时,设计上面需要注意哪些?不希望修改硬件参数。
2、12V供电,接入4Ω喇叭时,输出功率能达到多少?
3、如下如何理解,24V供电,功率也是6W?
4、TPA3113D2最大输出功率多少,即24V供电时候。
5、选用TPA3113D2时,喇叭该怎么配?10V供电,6w 8Ω测试效果最佳吗?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、12V供电,为了兼容2W 8Ω和6W 8Ω喇叭产品设计,当接入2W 8Ω喇叭时,设计上面需要注意哪些?不希望修改硬件参数。
您好,2W@8ohm喇叭,那么(0.707Vp)^2/R=2W, 可以计算得到Vp=5.66V。
根据Vp我们可以通过Vp=4*Plimit,计算得到Plimit的电压1.41V左右。
另外就是根据输出2W@8ohm,得到输出电流的大小,那么在设计输出滤波电路时保证电感的饱和电流要够大,否则会由于电感饱和导致烧坏。
2、12V供电,接入4Ω喇叭时,输出功率能达到多少?
输出功率和效率,THD+N,配置的PBTL还是BTL都有关系,建议直接参考数据手册中的P8-11的output power在不同配置下的曲线,其中包含了12V供电,18V供电,24V供电以及不同负载下的曲线。
3、如下如何理解,24V供电,功率也是6W?
测试条件是在THD+N=10%,f=1Khz,VCC=10V的条件下得到的连续输出功率为6W。
4、TPA3113D2最大输出功率多少,即24V供电时候。
24V供电,不同负载,不同测试条件下得到的输出功率不同,还是参考数据手册中的曲线表。
5、选用TPA3113D2时,喇叭该怎么配?10V供电,6w 8Ω测试效果最佳吗?
10V供电,如果输出能达到10V的话,则8ohm喇叭,输出功率为6.25W左右,考虑到效率,考虑到输出不一定能完全达到供电电压,建议适当提高供电电压。
可以通过设置Plimit的电压得到想要的输出功率。
测试的话,可以参考Table2的典型应用去配置。