This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM2706各引脚正常,但DA输出恒为VCC/2

Other Parts Discussed in Thread: PCM2706, OPA4134, OPA2134, PCM1794, PCM2706C

自供电模式,电源用两个LDO分别提供VCC_3.3和VCC_3.3_ANALOG

晶振为有源晶振,12脚(XTI)接晶振输出,13脚(XTO)悬空

D+的1.5K上拉电阻忘加了,后来在24脚(VBUS)和23脚(D+)之间直接焊上了一个0402的1.5K电阻

图中10uF的电容全部为X7R的陶瓷电容

接上电脑后成功识别,用foobar选中该设备并播放,能在D+和D-上看到信号,I2S输出也有信号,XTI和XTO都有12MHz的信号,PSEL FSEL DT TEST 电平均与原理图相同,/SSPND为高,VCOM为VCC/2,但VOUTL和VOUTR输出恒为VCC/2(只接了10k的电阻,后级没接)

从引脚上来看所有的设置都是正确的,PCM2706也换了3片,还换了一片PCM2707,I2S输出正常,/SSPND为高,代表芯片还是在正常工作的,可为什么DA就是没输出呢?

请各位帮帮我解决这个问题。谢谢。