原理图是按TI官方PDF资料设计的,GAIN=32db,输入电容4.7UF,主板电源接口是DC-005插座,外置通电的电源适配器插头插到主板DC005插座时,喇叭有很大的爆音,取下电源插头时也会有爆音(比通电爆音小一些),请教TI工程师,此爆音是怎样产生的?怎样消除爆音?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
原理图是按TI官方PDF资料设计的,GAIN=32db,输入电容4.7UF,主板电源接口是DC-005插座,外置通电的电源适配器插头插到主板DC005插座时,喇叭有很大的爆音,取下电源插头时也会有爆音(比通电爆音小一些),请教TI工程师,此爆音是怎样产生的?怎样消除爆音?谢谢
你好:
1.如果是单端输入,比较容易引起POP,POP是上电时,两端输入信号不匹配,不匹配信号被功放放大,在输出端即体现为POP——扑扑的声音。
2.POP最根本原因是输入端信号不匹配,例如正端和负端阻抗不匹配,输入电容器件的差异性等。
3.减小POP:
1)降低Gain,减小POP的放大倍数
2)减小输入电容,减小RC常数,电容充电的时间就会缩短,信号差异性就会减小。输入的两端尽量选用差异性小的电容。
3)合理控制上电顺序。
详细的请参见附件中的note。
你好:
通过更改掉电检测模块电路中的R1或R2阻值是能解决不同电压供电时的关机POP声。
是我的意思没描述清楚,我意思是不管供电电压是多少V,R1,R2阻值一定(量产时不会贴不同电阻的),掉电检测模块都会起作用。
你好:
这样的话,我觉得应该可以解决不同供电电压时的掉电检测的点的问题。但是5V稳压模块也许也有时延的问题,最终不知道效果会怎么样。
还有,我不太明白,量产的时候,你的产品电压供电是可调的吗?