This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助,TPA3116主板开关机爆音



原理图是按TI官方PDF资料设计的,GAIN=32db,输入电容4.7UF,主板电源接口是DC-005插座,外置通电的电源适配器插头插到主板DC005插座时,喇叭有很大的爆音,取下电源插头时也会有爆音(比通电爆音小一些),请教TI工程师,此爆音是怎样产生的?怎样消除爆音?谢谢

  • 你好:

    1.如果是单端输入,比较容易引起POP,POP是上电时,两端输入信号不匹配,不匹配信号被功放放大,在输出端即体现为POP——扑扑的声音。

    2.POP最根本原因是输入端信号不匹配,例如正端和负端阻抗不匹配,输入电容器件的差异性等。

    3.减小POP:

    1)降低Gain,减小POP的放大倍数

    2)减小输入电容,减小RC常数,电容充电的时间就会缩短,信号差异性就会减小。输入的两端尽量选用差异性小的电容。

    3)合理控制上电顺序。

    详细的请参见附件中的note。

  • 感谢Flora Wang 大侠的热心帮助,按你提供的PDF档中的电路手工搭焊了这个掉电检测电路,使用12V电源给系统和掉电检测模块供电,确实能解决关机POP声。

    但是有这样一个问题,TPA3116支持的工作电压范围很宽,12V时掉电检测模块作用正常,但如果用24V电源时关机POP声又会出现。

    分析掉电检测模块原理图,可不可以把掉电检测模块供电从PVCC断开,然后加入一个稳压电路,比如稳压5V,用稳压5V给掉电检测模块供电,不知是否可行?

  • 你好:

    电压升高了,改一下电阻,改一下掉电的保护点,应该可以解决这个问题吧。

  • 你好:

    通过更改掉电检测模块电路中的R1或R2阻值是能解决不同电压供电时的关机POP声。

    是我的意思没描述清楚,我意思是不管供电电压是多少V,R1,R2阻值一定(量产时不会贴不同电阻的),掉电检测模块都会起作用。

  • 你好:

    这样的话,我觉得应该可以解决不同供电电压时的掉电检测的点的问题。但是5V稳压模块也许也有时延的问题,最终不知道效果会怎么样。

    还有,我不太明白,量产的时候,你的产品电压供电是可调的吗?

     

  • 你好请问你是怎么个接法的,我的Q是405241165,麻烦加我,帮我解决一下这问题