Other Parts Discussed in Thread: TAS5711
我用CPU的引脚控制TAS5711的PDN引脚的电平高低,当我拉低PDN引脚后,TAS5711输出没声,达到静音效果,但是当我再次拉高PDN引脚时,输出不能恢复,还是没声,是否PDN引脚电平复位后,整个芯片需要重新RESET才能恢复工作呢?而不能单独使用PDN引脚拉高拉低来达到静音与非静音效果?请教TI的工程师解答,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
datasheet page 38和page39 推荐Power down后重新reset一下。重新上电,推荐按照datasheet的推荐上电时序工作。
power down是硬件shutdown,如果需要mute,可以写通过写寄存器0x6来实现。如需shutdown,还有软件shutdown,0x05寄存器。
Dear Flora,
还有一个问题,就是我在使用0X05寄存器的时候,第6位写1,SHUTDOWN静音之后,只把该寄存器的第6位写0,无法退出SHUTDOWN模式,必须把该寄存器直接写0X0,才能恢复声音,这样的话,我其它位写的数据又得在恢复声音后重新再写一次,请问0X05寄存器本身就是这样吗,芯片手册中写到“When bit D6 is set low, the system exits all channel shutdown and starts playing audio; otherwise, the outputs are shut down(hard mute)“,只说写第6位就可以了,在此很困惑,求解答