This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们目前在用TAS5825M这颗料,发现大功率输出的时候会保护,情况如下:
我们供电电压为24V,现在发现设置为768K,HYBRID模式连接8Ω电阻后输出功率稍微大点就会削波降低功率;
后面设置为768K,BD模式后连接8Ω电阻输出1KHz,25W不保护了,但是连接4Ω的时候设置输出25W就会保护;
之后设置为576K,BD模式后连接4Ω电阻输出1KHz,25W可以保持1到2秒就会保护;
之后设置为480K,BD模式后连接4Ω电阻输出1KHz,25W可以保持4到5分钟就会保护;
设置为384K,BD模式后连接4Ω电阻输出1KHz,25W不会保护;但是我们发现正常使用时设置为768K的时候电感和芯片的发热最小,现在我们想设置为高频率而芯片不会输出保护,请问是否有其他设置可以做到?
您好,
您是使用的自己设计的板子还是EVM板?
保护时建议您读下面fault寄存器,看是因什么进入了保护:
0x53h-D[6-5]寄存器设置的是什么?调制模式和开关频率需根据下表配合环路带宽配置:
过温保护机制测量的是die temperature,因此测量散热片温度是不准确的。
看下面链接中英文工程师给出的回复(Typically most significant difference can be seen between different modulation schemes but typically lower switching frequency offers better efficiency and higher loop bandwidth offers better performance.),也就是说降低发热功耗应从调制模式进行考虑,从datasheet 中9.4.6 Device Modulation章节看1SPW调制模式是最高效的,但有少量THD降级。
因此如果您想降低发热量且不损失THD性能,您可以考虑使用 Hybrid 调制模式,且选择较低的开关频率以提供更好的效率。
我们目前测试的是BTL,削波时的幅值大约7.5Vrms,削波到5Vrms或者更低,目前我们测试的是自己的板子,没有用PPC3配置:
在Hybrid模式下会削波降功率,BD模式下不会削波,但是比较容易出现过温保护,目前设置384K,BD模式不会保护,但是电感很烫,我们想通过配置其他模式改善发热问题,然后就出现了上面的现象。
为更加有效地解决您的问题,建议您将此问题发布在E2E英文技术论坛上,请资深的英文论坛工程师为您继续提供帮助。
英文论坛对应子论坛链接:https://e2e.ti.com/support/audio-group/audio/f/audio-forum
0x54的值我们配置了-3DB输出,值是6,这个在ppc3上面也有操作过,问题奇怪的是,在demo上面配置运行不会削波,用ppc3导出的表写到我们的板上就会削波,麻烦帮忙看看我们的设计是不是有什么漏洞还是有什么配置不对的地方?
最近通过飞线让PPC3来配置我们的板,发现用PPC3配置不会削波,用PPC3导出的表写入我们自己的板就会削波,目前还不知道问题出现在哪?下面为PPC3导出的表,也麻烦帮看看有没有问题,谢谢!384k+HYBIRD.txt
我想这可能与导出方法有关,下面链接是PPC3视频详解,其中前两个视频中有导出方法介绍,我不知道您是否已经观看,建议您观看下,看下导出过程是否有异常?
https://edu.21ic.com/lesson/2269