Hi TI engineer:
Our products have a small number of boot crashes in the process of customer use . But it didn't happen during production and testing, and more than 2,000 units of the product have been produced .
Here are some of our relevant parameters :
- power supplier:+24V Adapter
- load:8 ohm
- VC is from 24V,Series a diode and ground 100uF capacitor
question:
- the SDZ :What is the minimum time delay required for SDZ to be enabled during the power-on process?
- RINP/RINN: At the moment of power-on, there will be a pulse signal of about +12V in the signal input. Will this pulse signal cause input overload? So the chip crashes and burns?
- if the SDZ always high, when power on ,Will the chip crash?