This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3131D2: 音频功放概率性保护无输出

Part Number: TPA3131D2


    我司在调试1款对讲机产品时,使用TLV320AIC3106IRGZRcodec+TPA3131D2(音频功放)方案,发现音频功放会概率性保护导致输出异常,该功放电路及外围参数已大批量在其它机型使用,暂未发现问题,帮忙从原理图及PCB ,FAULTZ 管脚异常原因方面分析定位下可能的原因.

         异常时,FAULTZ信号异常,波形如上图所示

                           原理图文件

                       PCB及叠层

做过如下实验:

1.输出功率限制在3.5W,2.25W,1.64W,1.12W0.02W 问题依旧.

2.PVCC,增加10.1uF,11nf247uF,2470uF电容或使用外供电源,问题依旧.

3.SDZ信号做了如下验证,初步排除该控制信号问题

4.修改功放输出LC参数,选择合适的LC参数,可以规避该问题

5.不使用主板codec,使用外置音源(和幅度及频率无关),问题依旧;

codec输出信号连接到demon板(使用demon板功放),可以解决该问题.